FAQ

Q1

NOTE 1.1 Explanation of LED fundamentals

Ans

LED is a light emitting semiconductor device with diode-like characteristics. As forward current flows through the P-N junction of the semiconductor material, photons are released as a result of electrons moving across the diode and falling into the empty holes in the P-type layer. Depending on the photon’s frequency, it could either be invisible to the human eye (infrared portion) or be part of the visible spectrum. The lasted development in LED technology involves coating blue LED with phosphor to create white LED. 
The V-I curve of LEDs is similar to diodes. Please refer to figure 1.1


        Figure 1.1: LED V versus I characteristic 

White LEDs are generally used for lighting applications, the brightness of such device increases proportionally with the increase in forward conduction current.  Due to the rise in demand for high power, high luminance white LED in the lighting industry, specifications are being standardized. Forward voltage is typically within the range of 3.0~3.5V with forward current of 350/700/1050mA resulting in power rating of 1/2/3W.

Q2

NOTE 2.7 Adjustment of output voltage and current

Ans

Some MEAN WELL’s LED power supplies equip with functions of adjustable output voltage and current. Models with IP67 design (potted with heat transfer silicone) do not allow adjustment of output voltage and current, but HLG-150A/240A is with special design that allows external adjustment; for models with plastic enclosure, adjustment can only be made after taking apart the top cover. Adjustable voltage range will be +/-10% or +0/-15% of rated value and adjustable current range will be about 50~100% of rated value.
 

Q3

NOTE 2.9 Suggested solutions for EMC of LED luminaries

Ans

  •  Metal enclosure grounded to FG (Frame Ground):
  • For applications with FG connection, it is suggested to bond the metal cases of LED power supply and LED module to FG to reduce EMI (Electromagnetic Interference) of the whole system.
     
    •  Wiring:
  • Since the input and output cable length can be meters due to actual field applications, the common mode noise can be highly significant. To effectively reduce the noise, a clip-on common-mode core can be installed on the wiring close to LED module. This solution also applies if AC input cable is too long. Please refer to Fig.2.9 for illustration.
     
    •  High surge level requirement:
  • In order to meet requirement of surge level for outdoor applications, the surge immunity of HLG-60/100/150/240 is designed to be up to 4KV. For surge immunity of higher level, varistors or gas tubes (500V rating) can be installed in the outside of the power supply. But the configuration should also comply with requirements in safety norms. Please refer to Fig.2.9 for illustration.
     
                                            Fig.2.9: Illustration of suggested solutions for EMI and surge immunity
     
    • LED module with driver IC:
  • Since LED driver IC is a circuit topology employing high frequency switching (hundreds of KHz to several MHz), using it to deliver constant current to LED modules can complicate EMI debugging. Due to the EMI concerns, it is more than important to suppress the noise from driver IC. The PCB layout should focus on the size of driver IC’s ground trace and configuration of In/out capacitors and inductors. It is suggested that common choke, differential choke and high-frequency X capacitor should be incorporated into the PCB layout between the output side of power supply and the circuit of LED driver IC. Please refer to Fig.2.10 for illustration.



  •                                          Fig.2.10 Illustration of suggested EMI solutions for LED driver IC

     

    Q4

    NOTE 1.2 LED applications

    Ans

    Advantages of LEDs include low heat dissipation, diverse applications, miniaturization, high tolerance to shock/vibration, and ability to focus light beam.  The use of white LED in the lighting industry is accelerated by the continuing improvement in luminous flux and efficiency. Typical applications include building architecture (wall lighting, wall decoration, garden lighting, spot lighting, stairway lighting, and patio lighting), outdoor use (street light, park light, and lamp post), commercial use (office lighting, sign board, display cabinet lighting), and home use (cabinet lighting, room lamination, desk lamp, and etc).
     

    Q5

    Points on connecting wires used in power supplies?

    Ans

    To install a power supply into the system, you would need wires for the connection both to the loads and to the energy source. There are a couple of points that should be taken into consideration when choosing wires, one is current rating, it may cause high heat on the wires or burnt out in the worst case, if the rating is not enough. The other is voltage drop, there would be voltage reduction at load side as current moves through the wires owing to the internal resistance. If too much voltage drop in line, there could be no sufficient voltage to drive the loads. You can find the right wires for use by referring to the table below on the basis of your system design.

    Q6

    Why the input voltage marked on the spec. sheet is 88~264 VAC while the label on the power supply says that it is 100~240VAC?

    Ans

    During safety verification process, the agency will use a stricter standard -- ?0%(IEC60950 uses +6%, -10%) of the input voltage range labeled on the power supply to conduct the test. So, operating at the wider input voltage range as specified on the spec. sheet should be fine. The narrower range of input voltage labeled on the power supply is to fulfill the test standard of safety regulation and make sure that users insert input voltage correctly.

    Q7

    Notes on choosing a switching power supply?

    Ans

    1. To increase the reliability of the S.P.S., we suggest users choose a unit that has a rating of 30% more power than actual need. For example, if the system needs a 100W source, we suggest that users choose a S.P.S. with 130W of output power or more. By doing this, you can effectively boost the reliability of the S.P.S. in your system.
    2. We also need to consider about ambient temperature of the S.P.S. and whether there is additional device for dissipating the heat. If the S.P.S. is working in a high temperature environment, we need to make some derating to the output power. The derating curve of "ambient temperature" versus "output power" can be found on our spec sheets.
    3. Choosing functions based on your application:
          • Protection function: Over Voltage Protection (OVP), Over Temperature Protection (OVP), Over Load Protection (OLP), and etc.
          • Application function: Signaling Function (Power Good, Power Fail), Remote Control, Remote Sensing, and etc.
          • Special function: Power Factor Correction (PFC), Uninterruptible Power Supply (UPS) function.

         4.   Make sure that the model qualifies for the safety standards and EMC regulations you need.

    Q8

    Will MEAN WELL's products with CE marking meet the EMC requirements after assembling into my system?

    Ans

    We cannot guarantee 100% that the final system can still meet the EMC requirements. The location, wiring and grounding of the switching power supply in the system may influence its EMC characteristics. In different environment or applications, the same switching power supply may have different outcomes. Our test results are based on setup shown in the EMC report.

    Q9

    NOTE 1.3 LED lifetime and reliability

    Ans

    Since LED is part of the solid-state semiconductor device family, when properly designed-in, it has excellent lifetime and reliability figures. The lifetime of LED is typically between the range of 50,000~100,000 hrs. This exceeds the lifetime of the traditional lighting device (1,000~10,000 hrs) by a large margin. Extra attention must be given to cooling of LED and design of LED driver or else you risk premature failure and accelerated the decrease in luminance (refer to figure 1.2). The key to achieving energy conservation, high efficiency, and long lifetime is to select a suitable power source/drive method and provide proper cooling for the LEDs.


           Figure 1.2: LED junction temperature versus lifetime
     

    Q10

    NOTE 1.4 LED drive methods

    Ans

    The main factor to driving a LED is the introduction of forward current. However, due to its nonlinear V-I characteristic, high Vf manufacturing tolerance, and Vf sensitivity to temperature change, the most common types of voltage source used are limited to either constant voltage or constant current. The drawback of using constant voltage source is that LEDs will not produce the same brightness, resulting in uneven reliability, decrease in luminance and lifetime. For these reasons, the constant current voltage source is more preferable when it comes to driving high power LEDs. Just as named, the constant current source is not susceptible to the variations in forward voltage. Its current will remain at a constant level regardless of the shift in LED Vf. Thus, constant brightness can be easily achieved. Constant current can also be attained by using a driver circuit with current sense resistive network so no adjustment of the power supply voltage is required.
     

    Q11

    What is different between information (EN60950-1) and medical (EN60601-1) safety standard?

    Ans

    According to safety standard, the leakage current in EN60950-1 Class I cannot exceed 3.5mA; in EN60601-1 cannot exceed 0.3mA. Others criteria like safe distance and numbers of fuse are also different. Please consult the diagram below:

    Q12

    What is class 2, class II and LPS? What is the difference between class I and class II?

    Ans

    Class I: Equipment where protection against electric shock is achieved by using basic insulation and also providing a means of connecting to the protective earth conductor in the building where by routing those conductive parts that are otherwise capable of assuming hazardous voltages to earth ground if the basic insulation fails. This means a class I SPS will provide a terminal/pin for earth ground connection.
    Class II: Equipment in which protection against electric shock does not rely on basic insulation only, but in which additional safety precautions, such as double insulation or reinforced insulation are provided, there being no reliance on either protective earth or installation conditions. This means a class II SPS does NOT have a terminal/pin for earth ground connection.
    LPS: When an electronic circuit is powered by a limit power source (LPS), its output current and power are under the limitation shown in IEC60950-1 Table 2B, and the risk of fire can be reduced significantly. So, the safety distances and flammability rating of components can be much lower. Therefore, the plastic enclosure of these power supplies could use HB flammability rating to reduce cost. This definition comes from ITE product (IEC/EN/UL60950-1).

    Class 2: When an electronic circuit is powered by class 2, its output current and power are under the limitation shown in UL1310 Table 30.1, and the risk of fire can be reduced significantly. So, the safety distances and flammability rating of components can be much lower. Therefore, the plastic enclosure of these power supplies could use HB flammability rating to reduce cost. This definition comes from UL class 2 power unit (UL1310).

    Q13

    Why did the power supply shuts down during operation and after turning it off, I can restart the power supply again?

    Ans

    In general there are two circumstances that will cause the power supply to shut down. The first one is the activation of the over-load-protection (OLP). To deal with this situation, we suggest increasing the rating of the output power or modifying the OLP point. The second one is the activation of over-temperature protection (OTP) when the internal temperature reaches the pre-set value. All of these conditions will let the S.P.S. enter protection mode and shut down. After these conditions are removed, the S.P.S. will be back to normal.

    Q14

    NOTE 1.5 Introduction to Constant Voltage (C.V.) Mode and Constant Current (C.C.) Mode of LED Power Supply

    Ans

    Most of the traditional switching power supplies provide a constant voltage (C.V.) to the load. For example, MEAN WELL’s single output model RS-25-5 can provide 5V/0~5A to power all kinds of load. Its output voltage maintains at the constant value of 5V while its output current varies from 0~5A based on the load condition. When the loading is over 5A which is its rated current, the power supply unit will go into “overload protection” mode (generally speaking the activated range of overload protection is 105%~150% of rated output power). There are many different protection types that are often seen in the design of MEAN WELL power supply such as shutdown type (PSU will be shut off output), hiccup type (output voltage/current will be pulsing), and constant current type (output current will be fixed at a constant value between 105~150% of rated output current and the output voltage will go down to a low level). The power supply is under abnormal condition when the overload protection has been activated, so it is not suitable to let the power supply unit operate under this situation continuously. Equipped with “hiccup type” as their overload protection mode, the LPV, LPH-18 and LPL-18 series in MEAN WELL LED power supply family are considered to be “constant voltage power supply”. For LED related applications, it can be used in system incorporated with LED constant current driver IC (Fig. 1.5) or series connected with a ballast resistor (Fig. 1.4).





    The so-called constant current (C.C.) LED power supply basically refers to the “constant current protection” concept and its output current is maintained at a fixed value by means of feedback control (this fixed current level will be close to its rated output current). The only difference is : Under constant current (C.C.) operation mode (or constant current protection mode), the C.C. LED power supply is still within the normal operating range and all the components have been chosen to continuously provide this constant current output. Generally speaking, the power supply unit will operate under constant current region only when the system design belongs to “LEDs drive by the power supply directly” (Fig. 1.3).




                      Figure  1.6: Typical LED power supply I-V curve


    Fig. 1.6 is the I-V characteristic curve of a typical constant current LED power supply. The “constant current region” for each series of C.C. LED power supply may be different because of the different circuit design. As the figure shown above, the PSU will operate in the constant current region only when the output voltage is kept at 50% of rated output voltage or higher, so the sum of VF of all series connected LEDs should be higher than this limitation. If the sum of VF of all series connected LEDs can’t achieve 50% of rated output voltage, the power supply will go into the “hiccup region” and cannot drive the LEDs properly. Currently most of MEAN WELL’s LED power supplies can provide constant current output and the suitable operation region for directly connected LEDs is also specified in their SPECs (in the column of “Constant current range”). The constant current region can be 3V~100%VO, 9V~100%VO, or 70%~100%VO in different product series because of the difference of circuit design (concerning Harmonic Class C compliance, the lower limit may reach 75% of rated output voltage for some models with PFC function). When using power supply to drive LEDs directly, designer of lighting fixture should make sure that the VF sum of LEDs connected in series is high enough to operate the C.C. LED PSU in the correct region.
     
    In fact, MEAN WELL’s constant current LED power supplies also possess the feature of “C.V. + C.C.”. That means before reaching the “constant current region”, they can be operated within the “constant voltage region” just like traditional power supplies. In this region, system design must incorporate suitable “LED drive IC” or “series connected with a ballast resistor”; after entering the “constant current region”, the PSU can provide constant current as the output and hence can drive the LEDs directly. We can find that the “C.V. + C.C.” characteristic can be used in many different LED installations and make the system design more flexible.



    Below is the comparison chart of three different LED driving alternatives:

    Q15

    NOTE 1.6 LED lamp driver structure

    Ans

    The most often seen LED lamp setup is the series configuration because this ensures equal brightness to each of the LEDs. Even if the lamp consists of the same LED components from the same production lot there will still be slight differences in the forward voltage. As the working temperature increases, the LED forward voltage is bound to decrease leading to an increase in the forward current.  This is why it will be necessary to add the current limiting circuit to the LED setup.  The most common driving structures are as below: 

    • LED directly driven by a power supply Figure 1.7
    • This setup is the most cost-effective and wirings are simple. The designer will only have to worry about LED characteristics. Once that is taken care off, all the designer has to do is select a stable power supply with constant current limiting. However, there could still be issues with equal current sharing between each of the LED strings. Matrix LED structure can be used to minimize extensive damage from the
      failure of just a few LED. If a MEAN WELL constant current LED power supply is used to drive LEDs, the direct connection is possible and current limiting resistors and LED driver ICs are not required to somewhat balance the current flow to each LED string. However, the LED must be ranked in order to minimize large differences in Figure 1.7 combined VF of each of the LED strings which can lead to unbalance current flow to some of the strings and cause part of the LED structure to be damaged from the high current flow.

                         
                     Figure 1.7 Constant current power supply drive LED load directly
              
       
      • Series connection of LED current limiting resistor, refer to Figure 1.8 Series
      • The advantage of this architecture is that it is inexpensive and rather easy to assemble. Better balance in output current as compared to the direct drive method. The disadvantages are high power dissipation of these resistors, If current varies with the change in voltage, LED brightness may be uneven, cannot control current precisely and lack of protection for the LEDs.


                               
              Figure 1.8: Constant current or constant voltage power supply with LED driver resistor

            

        Example:
        The use of CLG-150-30(30V/5A) to drive 8 LEDs in series and 8 strings in parallel
         
           V    : LED power supply rated output voltage
           VF  : LED forward voltage (around 3.5V)
            IF:  : LED forward current (about 625mA)

             


         
          • Power supply in combination with linear driver IC, see figure 1.9​​​​​​​

        The cost of this structure is moderate. Other advantages include long lifetime for both LED and the power supply, simplicity of circuit design. Disadvantages includes higher cost as compared to using driver resistor with just as much power dissipation, and unsuitable for use with high tolerance voltage source.  
        Linear constant current driver can not automatically adjust the current flow to the LED. It does not balance current as well as PWM constant current driver. Its basic IC structure composes of resistor + electronic switch. LED drive current is regulated through the control of the switch’s conduction level.


          
        Figure 1.9: Constant current or constant voltage power supply with linear LED driver
          • Power supply in combination with PWM constant current driver IC, see figure 1.10
        This structure is the mainstream driving method preferred by most LED lighting manufacturer. The main reasons are steadiness of current control and even current sharing. Other advantages include long lifetime for both the LED and the power supply. Disadvantages include higher cost as compared to other driving methods, complicity in connection, the PWM driver can cause EMC interference and produce high frequency audio noise.
        The PWM constant current driver will automatically adjust current flow to achieve balance in current for each LED string thus insure each branch has equal brightness. Main topologies include buck, boost, and buck-boost. Either pulse width or frequency is modulated to maintain constant current.

           
        Figure 1.10: Constant current or constant voltage power supply with PWM constant current LED driver

    Q16

    What should we pay attention to if system implemented magnetic component?

    Ans

    Nowadays, customer implement magnetic component in their system to achieve fast installation and maintenance. The magnetic component should keep as far as possible from PSU to avoid interference in the control circuitry of PSU. If limitation of distance is unavoidable, install a well magnetic-conducted metal plate (ex: steel plate, copper plate) between PSU and magnetic component to minimize the interference.

    Q17

    What is SELV for information products?

    Ans

    This regulation applies to the secondary circuitry. The circuit should be designed to guarantee that under normal operating conditions, the voltage between any two touchable points should be less than 42.4Vpeak or 60Vdc. For class I equipment, it refers to "between any touchable point and the ground." Under single fault conditions, the voltages between any two conductors of the SELV circuit and between any one such conductor and earth shall not exceed 42.4V peak or 60Vdc for a period longer than 0.2 seconds. Moreover, a limit of 71V peak or 120Vdc shall not be exceeded. According to requirements below, MW SPSs can comply with SELV. IEC 60950-1 (ITE SPS): voltage of o/p circuit is less than 60Vdc under normal condition. IEC 61347-2-13 (LED SPS): voltage of o/p circuit is less than 120Vdc under normal condition.

    Q18

    What is "Inrush Current"? What will we notice?

    Ans

    At input side, there will be (1/2 ~1 cycle, ex. 1/120 ~ 1/60 seconds for 60 Hz AC source) large pulse current (20~100A based on the design of S.P.S.) at the moment of power on and then back to normal rating. This "Inrush Current" will appear every time you turn on the power. Although it will not damage the power supply, we suggest not turning the power supply ON/OFF very quickly within a short time. Besides, if there are several power supplies turning on at the same time, the dispatching system of AC source may shut off and go into protection mode because of the huge inrush current. It is suggested that these power supplies start up one by one or use the remote control function of S.P.S. to turn them on/off.

    Q19

    What is LPS ? If the power supplies can meet LPS, what is the benefit for the end product?

    Ans

    The requirement of LPS is from IEC60950. It means the product output shall not exceed 60V/8A/100W under the normal and abnormal condition.
    If the power supplies can meet LPS , the end product does not need the fire enclosure.

    Q20

    NOTE 2.1 Instructions on Assembly

    Ans

    • As step 1 shown in figure 2.1, connect LED luminaries to the output cable of Mean Well LED power supply.
      • As step 2 shown in figure 2.1, connect the input cable of Mean Well LED power supply to AC mains.


    • ! CAUTIONS: Step 1 should always come before step 2. If step 2 comes first, a high transient surge current will go into the LED luminaries and it can damage LEDs in an LED luminaries without LED driver IC.



       Fig.2.1: Assembly of LED power supply


         

    Q21

    NOTE 2.3 Effect of output load on efficiency

    Ans

    The types and levels of output load have significant effects on the efficiency of a power supply when operating at normal conditions. The chart below presents the change of the efficiency of HLG-150-36 operating at 70~100% LED load and 70~100% general load, and indicates that the efficiency will be lower as the total Vf (forward voltage) of LEDs in series is lower when LEDs are directly powered by LED power supply. Therefore, it is a better design to set the total Vf of LEDs in series at 85~95% of the rated voltage of the power supply.



     

    Q22

    What is LVLE ? If the power supplies can meet LVLE, what is the benefit for the end product?

    Ans

    According from UL8750 definition below:
    a. 0-30Vdc output voltage: Maximum 8 amps
    b. 30-60Vdc output voltage: 150/V amps
    If the power supplies can meet LVLE , the end product does not need the fire enclosure.
     

    Q23

    What is MOOP and MOPP?

    Ans

    a. MOOP: provide adequate protection to the operator
    b. MOPP: provide adequate protection to the patient
    c. MOP: only one protection
    MW products declare 2 MOPP means that MW product can provide two adequate protections to the patient.
    It minimum the risk and also suitable for the patient.

    Q24

    Requirements on parallel operation?

    Ans

    When power supplies are connected in parallel, it is able to increase the output current or use them as the redundant (back-up) function. Be sure that the difference in
    output voltage and wiring impedance should be small when operating in parallel.
    1. Connect P(LP/CS) terminals together such as the PSP models (Please refer to the parallel function of specification). Input and output should be connected in parallel before connecting to the AC source and loads. Shown as in picture below (some S.P.S. require a minimum load after paralleling).


    2. Output voltage difference between S.P.S. units should be as small as possible, normally < 0.2V.
    3. The power supplies should be paralleled with short and large diameter wiring together first, and then connected to the load.
    4. After paralleling, the maximum usage of total power should be around 90% of the rated total power.
    5. When power supplies are paralleled, if the load is lower than 10% of rated load of individual S.P.S. The LED indicator or signals (Power Good、Pok、Alarm Signal) may malfunction.
    6. To ensure that the load current is effectively shared in parallel operation, in general, it is recommended not to use more than 4-6 power supplies at one time.
    7. In some models, the +S, -S terminals should be used to reduce unstable pulsation of output voltage.

    Q25

    NOTE 2.2 Protection function

    Ans

    All of MEAN WELL’s LED power supplies are designed with protection functions against inrush input current, peak input voltage, short-circuit at output, overload (OLP) at output and over voltage (OVP) at output. Some models also equipped with over temperature protection (OTP). Please refer to Mean Well’s switching power supply technical manual for detailed information.
     

    Q26

    NOTE 2.4 Effect of output load on power factor (PF)

    Ans

    The effect of different types of load on power factor (PF) and the harmonic current is as shown in the chart below. The power factor of MEAN WELL’s LED power supply operating at LED load will be lower than at general load, and the total Vf level of LED in series will also affect power factor. Therefore, it is a better design to set the total Vf in LED luminaries close to the rated output voltage of the power supply.


    Q27

    There is a definition of SELV in IEC61347. Is it the same with IEC60950?

    Ans

    No, they are different. SELV means the LED driver will use a safety isolating transformer with double or reinforced insulation and the output voltage shall not exceed 120Vdc.
    This is good for the end product safety certified if the LED driver with SELV output.

    Q28

    What is Type HL?

    Ans

    The requirement of Type HL is from UL8750. It provide one option for evaluation of LED drivers that are intended for use in a Class I, Division 2 hazardous location luminaires.
    It is simplify the procedure for the manufacture to apply the explosion-proof luminaires.

    Q29

    NOTE 2.5 Comparison of circuit topologies with power factor correction (PFC) function in LED power supply

    Ans

    MEAN WELL’s LED power supplies equipping with power factor correction function mainly adopt the two kinds of circuit topologies below. A Comparison between circuit topologies with and without PFC function is shown as the table below.



                                             Fig.2.2: Block diagram of non-PFC circuit topology


                                          Fig.2.3: Block diagram of circuit topology with single stage PFC


                                     Fig.2.4: Block diagram of circuit topology with two-stage PFC


    Q30

    NOTE 2.6 Heat dissipation of LED

    Ans

    LED is actually not with high luminous efficiency. Only 30% of supplied power is converted into visible light; the remaining of 70% is lost as heat. Due to this, thermal design plays an extremely important role in LED applications. According to the temperature characteristics of LED, luminous flux will attenuate by 3% and reliability will decrease by 10% for every temperature increment of 5℃ on LED. Therefore, temperature rise of LED is the major factor in life time and light loss.

     

    • All of MEAN WELL’s LED power supplies adopt thermal design of free air convection. Maximum operating temperature can reach 50℃~70℃. In addition, the metal enclosure of CLG series is able to release the heat through system case in where CLG series is installed, so as to improve system reliability.
    •  The life time of LED power supply is highly relevant to operating temperature. Take HLG-150 as example, for operations at the same load level, the lower the operating temperature, the longer its life time; for operations at the same operating temperature, the lighter the load, the longer its life time. When choosing a power supply, it is recommended to add a margin to the actual power usage to match the longer life time characteristic of LED. The relationship is as shown in Fig.2.5.


                           
    Fig.2.5: Relationship between output load, operating temperature and life time in LED power supply
    • In Fig.2.6 (de-rating curve for HLG-150), in order to avoid high temperature rise and maintain the reliability of the power supply, the rated power capability needs to be de-rated when ambient temperature exceeds 60℃ for operation at 230Vac input. Due to the abovementioned, the management of operating temperature should be taken into consideration in system design.

                     Fig. De-rating curve for output load against ambient temperature in LED power supply

    Q31

    What should be noticed when installing a power supply in vertical and horizontal directions?

    Ans

    Most small wattage and fanless power supplies are mainly installed in the horizontal position. If you have to install it vertically because of mechanical limitation, you should consider the output derating due to the heat concern. The temperature derating curve can be found on the spec sheet. Regarding the power supplies with built-in fan or the application has forced cooling system, vertical and horizontal installations have less difference. Ex. In SP-150 derating curve, the ambient temperature difference in application is 5 Celsius from vertical to horizontal. The output wattage in forced cooling can be 20% higher than air cooling convection.

    Q32

    What are the protection forms of overload/overcurrent?

    Ans

    When current drawn exceeds the rating of the PSU, the protection circuit will be triggered to protect the unit against overload/overcurrent. 
    Protections of overload/overcurrent can be divided into several forms:
    (1)FOLDBACK CURRENT LIMITING
    Output current decreases about 20% of rated current, shown as curve (a) in the figure below. 
    (2)CONSTANT CURRENT LIMITING
    Output current remains at a constant level and within the specified range while the output voltage drops to a lower level, shown as curve (b) in the figure below. 
    (3)OVER POWER LIMITING
    Output power remains constant. As output load increases, output voltage decreases in proportion, shown as curve (c) in the figure below.  
    (4)HICCUP CURRENT LIMITING
    Output voltage and current keep pulsing ON and OFF repeatedly when protection is activated. The unit automatically recovers when faulty condition is removed.
    (5)SHUT OFF
     Output voltage and current are cut off when output load reaches protection range. 
    NOTE: Protection mode of some of the products combines with different types of the forms mentioned, such as constant current limiting + shut down.

    Recover method:
    (1)Auto Recovery: PSU recovers automatically after faulty condition is removed.
    (2)Re-power on: PSU restarts by manual AC re-power on after faulty condition is removed.
    Note:Please do not operate PSU in overcurrent or short-circuit condition for a long period of time to prevent a shorten lifespan or damaging the PSU.

    Q33

    How to find products you need in MEAN WELL website?

    Ans

    Click “Products” on the website Menu. Four methods are provided to search MEAN WELL power supply products.
    1. Series Search
        Click “product style” such as DIN Rail, LED Driver or Charger, and you can rapidly find the corresponding
        product series. Through wattage and function information, you will find the products you need.
    2. Quick Search
        By choosing product type and electrical characteristic, related power supply and specification are shown
        below.
    3. Product Search
        It's classified by the application type, such as Parallel Series, Medical Type, and DC/AC Inverter. Choose
        the function or characteristic, and you can find the related products and specifications.
    4. Direct Search
        If you know the series name, click “magnifier” icon from the upper right of MEAN WELL website, and type
        the complete or part name to search the related product information.

    Q34

    What product information does MEAN WELL website provide?

    Ans

    The product information shown on MEAN WELL website is as below.
    1. Specification
        Details of product features, electrical specification, function, and mechanical specification can be found in the specification page.
    2. Test report
        The report content includes design verify test, safety & EMC test, and reliability test, ensuring the user safe through inspection,
    3. Certificate
        The certificate from accredited certification body is provided for customers' reference.
    4. User manual
        User manual provides detailed product instruction and considerations.

    Q35

    If the suitable product cannot be found, how to contact MEAN WELL?

    Ans

    You can send your product demand to local distributors at first, and the distributors can provide immediate service and suggestion. Besides, you can find “Contact Us” on website to fill out Sales Inquiry Form and we will reply your query promptly.

    Q36

    How to know the product discontinued information?

    Ans

    Providing the best price-performance ratio of standard power supplies and services are MEAN WELL enterprise mission. To comply with the latest updated international safety regulations, MEAN WELL develops the corresponding new high cost-performance products. Through “Products”, you can see “Not Recommended for New Design” and “Discontinued Products”. The former one shows models which will be gradually discontinued and replaced in the future. The latter one is models that are going to be discontinued and EOL.

    Q37

    What is the purchasing channel for MEAN WELL products?

    Ans

    For small and medium quantity demands, local distributors offer better price and enough stock for your timely delivery. However, for further contact to MEAN WELL, please fill out “Sales Inquire Form” in the “Contact Us” page, service will be offered promptly.

    Q38

    How to know MEAN WELL distributors information?

    Ans

    MEAN WELL has authorized distributors all over the world. You can find “Distributors” to search local distributors by area and product type. Our distributors will surely provide high quality service.

    Q39

    How to learn MEAN WELL new product launching announcement?

    Ans

    MEAN WELL develops new products constantly. Click “New Products” in “News” page for acquiring complete model information and key features.

    Q40

    Where to find the product test report?

    Ans

    To discover product complete test reports, click product information link and the report shows various information, such as electrical characteristic, protection, control function, stability, safety, and EMC.